- If the Home and End sensors of the motor are used, it is not possible for the rotary actuator to have a movement that is larger than 360 degrees, and have it come back to the starting position without being stopped by the endstop sensors.
- If a movement of more than 360 degree and return to starting position is needed, both endstop sensors must be disconnected.
- If the movement of more than 360 degrees and return to starting position is required, together with a homing functionality, a sensor that is connected to an IO module will need to be used as a home sensor with custom programming through Python.
Comments
0 comments
Please sign in to leave a comment.