Home› machine-builder

machine-builder

Discussion List

  • Sean Wilson
    Making a counter that monitors input in the background of a MachineLogic app and preforms an action
    Preface: This is presented solely as information. Use it at your own risk. The visual references in this discussion are screenshots from Machine Logic (as of 8/28/20) inside the online environment of 3D Machine Builder and may display options that are not available or are named differently then wh…
    Sean Wilson 31 views 0 comments 2 points Started by Sean Wilson August 2020 MachineLogic
  • Vention Demo
    Include add-on components to your design
    Include add-ons in the MachineBuilder to ensure you have all the necessary tools and consumables to assemble your design: [1] Click on "Add-ons" at the bottom left of the MachineBuilder: [2] Click "+" or "-" to adjust the quantity of tools and consumables: [3] Click &q…
    Vention Demo 16 views 0 comments 0 points Started by Vention Demo August 2020 MachineBuilder
  • Vivian Cheung
    Simulate your design in MachineLogic
    Once you have completed your design in MachineBuilder, try simulating your automated equipment using MachineLogic. This allows you to validate the operation cycle, correct the placement of sensors, and utilize a code-free program (MachineLogic) on your MachineMotion controller to operate your equip…
    Vivian Cheung 12 views 0 comments 0 points Started by Vivian Cheung August 2020 MachineLogic
  • Jennifer Sewell
    Resizing extrusions in MachineBuilder
    Once your extrusion is connected you'll have the additional option to resize its length. This feature is also available for linear axis' and belt conveyors. Once selected, click the “resize extrusion” icon on the navigation compass.  An "arrow-handle" will appear at either end of the extr…
    Jennifer Sewell 19 views 0 comments 1 point Started by Jennifer Sewell August 2020 MachineBuilder
  • Jennifer Sewell
    Inserting & connecting parts in MachineBuilder
    To add a part to your design, click on the desired part in the parts menu Then click into the 3D workspace to drop the part at the desired location. This is where the term ‘click-and-click’ interface comes from. To connect parts add the part to the 3D workspace and bring it to where you wish to ma…
    Announcement Jennifer Sewell 9 views 0 comments 1 point Started by Jennifer Sewell August 2020 MachineBuilder
  • Jennifer Sewell
    Step-by-step guidance for complex components with configuration engine
    The Configuration Engine provides users with step-by-step guidance for complex components. It lets you configure a fully functional linear actuator, conveyor, and pneumatic system, from motor selection to sensor, to related accessories. Once a first part is selected, the configuration engine is a…
    Announcement Jennifer Sewell 2 views 0 comments 1 point Started by Jennifer Sewell August 2020 MachineBuilder
  • Jennifer Sewell
    Simplify assembly with Automated Assembly Drawings
    Design your manufacturing equipment online and automatically generate step-by-step assembly instructions, in seconds. Assembly drawings can be understood by anyone with a general technology background.
    Announcement Jennifer Sewell 41 views 0 comments 0 points Started by Jennifer Sewell August 2020 MachineBuilder
  • Jennifer Sewell
    Define project parameters and automated processes with MachineScope
    With MachineScope, users can define their project parameters and automated processes, create end-to-end equipment requirements, and even establish their acceptance criteria.  MachineScope is also collaborative. It is digitally integrated in the Vention technology stack, where collaborators can easi…
    Announcement Jennifer Sewell 6 views 0 comments 0 points Started by Jennifer Sewell August 2020 MachineBuilder
  • Jennifer Sewell
    Simplify design using shortcuts and step-by-step instructions with MachineBuilder Instructor
    If you're new to MachineBuilder or interested in becoming a power-user, the Instructor will guide you through the platform. Shortcuts and step-by-step instructions help orient you to MachineBuilder's functions and features. The instructor also helps you to learn about the different hardware and ho…
    Jennifer Sewell 3 views 0 comments 1 point Started by Jennifer Sewell August 2020 MachineBuilder
  • Adeola Odusanya
    NEW: Instructor Pane in MachineBuilder
    Democratizing industrial automation starts with simplifying the design process. This is why MachineBuilder just got even easier to use. To help you build your automation project faster, we've added a virtual assistant to guide your design journey. Instructor Pane Toggle the instructor pane to ON (…
    Announcement Adeola Odusanya 12 views 0 comments 0 points Started by Adeola Odusanya July 2020 MachineBuilder

New to the community? Start here!


Join the community

It looks like you’re new here. If you’d like to join the discussion, click one of the buttons below!

Sign In Register

Quick Links

  • Categories
  • Recent Discussions
  • Activity
  • Best Of...
  • Unanswered