MachineFrame
Archives for August 2020
Discussion List
-
Ways to create a door on VentionThere are several ways to create a door, depending on the configuration desired. Here are some of my examples, if you have any others please share them here! (e.g., bifold doors) Enclosure with Single Inside Door: https://vention.io/designs/enclosure-with-single-inside-door-77958 Enclosure with Sin…
-
Can I have a specific extrusion size?Vention standard length increments are 45mm, which is how we can ensure rapid delivery times as we keep all of them in inventory. Custom or specific extrusions sizes are possible, however. It’s a manual process that will include an additional fee, and it also requires the intervention of an AppEng…